What is the definition of a STM32 project from a path/directory point of view?
I am new to STM32 products and development software. I have purchased the STM32F303RE Nucleus-64 Eval Brd. I'm also using SW4STM32 IDE as there are more examples. I have had some success, I still have some fundamental questions. I also downloaded and installed the STM32CubeF3 package. Within the "CubeF3" I was able to BUILD and run the GPIO_EXTI and download to target board. Wanting to make sure I understood the flow and file names, I went back using UM1766, PG 18 to load the next example GPIO project (GPIO_IOToggle). I flip the page UM1766, PG 19 as I'm using SW4STM32, this page states I go to the "workspace directory". Item (d) - PG 19 states browse to workspace directory and select project. My concern is; UM1766 Pg 15, under the EXAMPLE FILE STRUCTURE shown , there is no WORKSPACE in this file structure.
In order to load the PROJECT I had to go ALL the way into folder "GPIO/GPIO_IOToggle/SW4STM32" to load the project and note sure what I loaded. Note, no workspace was entered. Yes, I was able to load the PROJECT and BUILD. My question is what FILE in the final folder is the PROJECT file? Typically a software tool system will exist under a GLOBAL PROJECT file name, e.g. NAME.PRJ. This is important to know as the next step in UM1766, PG 19 is "DEVELOPING YOUR OWN APPLICATION" - . The engineer should know the definition of a PROJECT STRUCTURE and it's NAME. So my question is, what is the GLOBAL umbrella file for all the files that live under and in the 'SO CALLED" project space.
Is there one, or just a GROUP of files?