Skip to main content
EQuac
Visitor II
August 21, 2019
Question

STSW-PLM2GUI not working

  • August 21, 2019
  • 1 reply
  • 705 views

Hi all,

I'm trying to use the X-NUCLEO-PLM01A1 expansion board with the NUCLEO-F401RE board. I've been following the instructions to bring it up, and one of the instructions was to install the STSW-PLM2GUI to be able to interface the boards with the EVALKITST7580-1 GUI. However, after installing the software the GUI looks different from the one shown in the datasheet, and any attempts to connect to the board results in the message "SM : Status Message not received, check for connections". Additionally, running the P2P demo code on the board causes a "Warning: non STX character received" message to appear repeatedly, although the data is readable over PuTTY. I've noticed the version of the GUI is ST7580 GUI R21 (2017/08/04) while the datasheet shows X-NUCLEO-PLM01A1-7580 GUI R20 (2017/05/18) which I have not been able to find anywhere online. Can someone help me find the correct version of the GUI or get the one I have to work properly?

This topic has been closed for replies.

1 reply

FSiem.2
Visitor II
May 8, 2020

Hi all,

I had the same problem. I made the following adjustments:

  • other Win-Driver (W7-64) STSW-STM23102 -> STSW-LINK009
  • GUI: X-NUCLEO; Baud rate: 115200