Where are the DEMO source project file for the OUT OF BOX demo for the Nucleo-64 STM32F303RE board.
I purchased a Nucleo-64 STM32F303RE for beginning a project. I have downloaded the tools, this includes CUBE_MX and CUBE_IDE. I am able to build a project using these tools as instructed. What I want to know is where is the DEMO project that is loaded on this board straight out of the box. I was able to locate the HEX file on the ST Website; the only way I knew this HEX file was the one in the eval board is by reading the README.file. I was able to press the USER button and change the BLINKY LED rate. I would like to download the source file as I want to see how the HAL_FUNCTIONS were used. I won't download a new compiled HEX as the original will be overwritten and gone. I looked everywhere. Please help.