Skip to main content
victor.b
Associate II
Aug 13, 2019 6:54 PM UTC
Solved

Why is cubeprogrammer using a GUI installer on linux!?

I am on windows 10 and would like to use sub-system for linux (WSL) to cross-compile OpenST. So far i made it trough all the steps...until i saw that the cubeprogrammer is using a GUI installer...witch doesnt work on WSL....

Are there plans to make that cubeprogrammer available in "non gui" installer?

Thanks

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Sep 2, 2019 9:18 AM UTC

Hi @Community member​ 

STM32CubeProgrammer "non gui" installer is plan for first half of 2020.

In the mean time you can use version installed on the native Windows to flash files generated with WSL.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

4 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Sep 2, 2019 9:18 AM UTC

Hi @Community member​ 

STM32CubeProgrammer "non gui" installer is plan for first half of 2020.

In the mean time you can use version installed on the native Windows to flash files generated with WSL.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
VBurs
Associate III
Jul 31, 2020 5:59 PM UTC

Hi,

We are now past the mid of 2020 and i don't see any way to install STM32CubeProgrammer from the command line entirely in linux.

Is there any news about the release date?

Victor

Ozone
Principal
Sep 11, 2019 9:07 AM UTC

In the meantime, you could use a Linux distribution of your choice in a VM, like VMPlayer.

VBurs
Associate III
Jul 31, 2020 6:00 PM UTC

Hi Ozone, it is not an option because we use TouchGFX from ST and it is only compatible with windows...