2019-08-12 2:15 PM
i checked databook , but couldn't find out the maximum value of HAL_VTimerGetCurrentTime_sysT32();
if it's maximum value is max value of uint32_t? (i.e. 4294967295)
besides, how to restart the virtual timer?
2019-09-05 7:35 PM
HAL_VTimerGetCurrentTime_sysT32() returns a 32bit absolute current time expressed in internal time units.
To convert the internal time units to milliseconds, please call HAL_VTimerDiff_ms_sysT32()
The code would be something like:
time_ms = HAL_VTimerDiff_ms_sysT32(HAL_VTimerGetCurrentTime_sysT32(), 0);The maximum value is 4294967296, which is approximately 174 minutes.