Question about choosing 32MHz HSE quartz crystal
Hello I am going to use STM32WB55Vx for my aplication and have a question about choosing 32MHz HSE quartz crystal.
The document "AN5042 HSE trimming for RF applications using the STM32WB Series" determines Gm ( the transfer conductance of the HSE amplifier ) as vlaue from 0.18 to 2.84 mA/V. For stable operation, I have to chose 32MHz quartz crystal with Gmcrit ( minimal transconductance of an oscillator) is 5 (GAINmargin) times smaller (acording to AN2867 Oscillator design guide for STM8AF/AL/S and STM32 microcontrollers). The crystal NX2016SA 32 MHz EXS00A-CS06654 (from AN5042) has parametres: Cl =8pF, Co~ 1pF, ESR = 60 Ohm so Gmcrit ~= 0.6366 and GAINmargin =4.46 for the greatest Gm 2.84 mA/V.
I think it is difficult to find oscillator for GAINmargin>= 5 taking into account embedded capacity bank 12-16pF HSETUNE[5:0].
Сan confirm operation for GAINmargin values below 5? What is mimum GAINmargin for STM32WB?