2019-08-08 2:01 AM
Hello. I am using the SPV1040 solar boost converter within the STEVAL-ISV012V1 development board. The datasheet states that the converter can work with an input voltage as low as 0.3 V. The solar cell I am using is able to provide 0.6 V (Voc) and 100 mA (Isc), but the voltage output is never stepped up using this low input voltage.
I have tried even connecting directly a power supply as if it was the solar panel, and the output voltage only steps up with input voltages greater than 0.85 V. Should I change any component in the design to achieve boosting from inputs as low as 0.3 V, as stated in the specifications?
Any help would be highly appreciated!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.