cancel
Showing results for 
Search instead for 
Did you mean: 

hi there, need the c code to use UART protocol on X-NUCLEO-NFC03A1 RFID Reader with the STM32MP157-dk1 develeopment board

Gchri.0
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

as of today, there is no port of the ST25R95/CR95HF on STM32MP1xx. Anyway there is an existing non-official port on Linux for Raspberry Pi that might be used for porting on STM32MP1xx. See CR95HF - Linux RFAL demo.

Note: the communication protocol in the CR95HF - Linux RFAL demo is SPI. I would personally recommend to use SPI rather than UART.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

as of today, there is no port of the ST25R95/CR95HF on STM32MP1xx. Anyway there is an existing non-official port on Linux for Raspberry Pi that might be used for porting on STM32MP1xx. See CR95HF - Linux RFAL demo.

Note: the communication protocol in the CR95HF - Linux RFAL demo is SPI. I would personally recommend to use SPI rather than UART.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.