USB shows up as an "Unknown device (port Reset Failed)"
I am trying to get the STM32F722 to interface with the USB3300 external HS PHY (ULPI).
I have generated code from the cube.
I been doing digging..
the "USBD_CDC_Init" function never get called and pClassData is always NULL.
I have tried changing the HEAP and STACK sizes. (to 0x1000, 0x800 base on reading the forums)
Hardware seems to be correct: clocks, voltages 3.3v & 1.8v, etc
I tried different USB cables also base on reading the forums.
Need advice what to check next...?
Thanks
Greg
STM32F22RC
TrueStudio 9.3
STM32CubeMX 5.3
Cube package: STM32F7 v1.15.0