Skip to main content
virtex
Associate
July 29, 2019
Question

Strange behavior writing to external SRAM

  • July 29, 2019
  • 3 replies
  • 993 views

I have a STM32H753 with 16MByte, 32bit SDRAM​ and a Wiznet W5300 in 16bit mode (acts as SRAM Bank 1, SRAM_BANK_ADDR = 0x60000000).

So, if I read a Memory cell:

uint16_t aw = *(volatile uint16_t*)(SRAM_BANK_ADDR);

all is ok. With a scope on NE1, NOE, NWE I got one read cycle on line NOE.

But if I write to the Memory cell:

*(volatile uint16_t*)(SRAM_BANK_ADDR) = 0x8000;

I got four write cycles (shown on scope).

Going down to 8bit bus width, I got 8 write cycles.

This makes the W5300 confused.

But if I modify the Memory cell within the Debugger (Keil + ST-LinkV2, Memory Window)

I got one write cycle (as I expected).

Same code executed on a identical board assembled with a STM32F439 works perfect,

one write cycle as expected.

Does somebody has any idea to solve this Problem?

Best regards

Christian

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
July 29, 2019

How's caching set up for that area in MPU?

JW

virtex
virtexAuthor
Associate
July 29, 2019

​I think Cache is disabled and commented out. Or is there any other Cache enabled by default on power up?

 /* Enable I-Cache---------------------------------------------------------*/
 //SCB_EnableICache();
 
 /* Enable D-Cache---------------------------------------------------------*/
 //SCB_EnableDCache();

I am new on this device. We used the STM32F439 before. The Manual of the H7 device have twice the amount of pages of the F439 device.

So I am (not) familiar with all details of this device.

I think there is a relation between AXI buswidth (64 bit) and connected Memory. One write command generates 64bit/MEMBUSWIDTH writepulses on the NWE-line.

But why can I write to a single Memory cell with the Debugger?

Best regards

  Christian

waclawek.jan
Super User
July 29, 2019

> is there any other Cache enabled by default on power up?

I don't know. I don't use the 'H7.

> The Manual of the H7 device have twice the amount of pages of the F439 device.

That's no excuse. ;)

And you should add all the pages of the generic Cortex-M7 documentation.

0690X000009Za76QAC.png

> I think there is a relation between AXI buswidth (64 bit) and connected Memory.

Well spotted.

From Supported memories and transactions subchapter of the FMC chapter:

The memory region MPU attribute must be configured as “Device�? or “strongly-ordered�?

in order to prevent issues on devices that do not have the byte select feature. As an

example, if byte accesses are performed to 16-bit memories with the MPU attribute set

to “Normal memory�?, the AXI transaction size is 64 bits and the FMC splits the

transaction into four consecutive accesses while only one access is expected instead

of four.

> But why can I write to a single Memory cell with the Debugger?

Debugger may have it's own way to access the buses. Again, I don't use the 'H7 nor any Cortex-M7 device so I'm not familiar with the intimate details of its architecture.

0690X000009Za5KQAS.png

JW