DAC peripheral on STM32F407
I am working with STM32F407VG microcontroller (STM32F4 discovery board). When using the DAC peripheral for an application I was verifying the minimum and maximum voltage that can be generated from the DAC pin by providing values of 0 and 4095.
However the minimum and maximum should be within VSSA and VDDA even in case of VREF+ given to VDDA.
But when setting the DAC value to 0, I receive 50mV on the scale of 0 - 2.9 V and 61mV on the scale of 0 - 3.26V.
As per my understanding I thought I should be getting 0-1mV when DAC value is set to 0.
I have no other peripheral initialized or connected any other board to discovery board.
Can someone please tell me reason for its behaviour?