TI3 and TI4 mapping on input capture
I'm just setting up the input capture on timer 2, input capture 4. On page 411 of the reference manual for the CCMR2 register and the CC4S bits, it states "01: CC4 channel is configured as input, IC4 is mapped on TI4 10: CC4 channel is configured as input, IC4 is mapped on TI3".
I'm not sure what TI3 and TI4 are referring to. I've done a search and this is the only place they are mentioned.