Skip to main content
wouter.kiesewetter
Visitor II
July 22, 2019
Question

Change memory map of application using STM32CubeMX

  • July 22, 2019
  • 0 replies
  • 732 views

Hello,

For a project generated with STM32CubeMX I have to update the memory map in the linker file to be able to use it with a bootloader. The linker file is generated by CubeMX but I don’t see an option to define the starting address of the application in flash. The default address is 0x08000000 but I want to change it to a higher value.

My question is: How can I configure a different starting address of the firmware in flash?

If that option is not available in CubeMX I would like to know how I can exclude the linker file from being overwritten when the project is regenerated.

The STM32CubeMX version used is 5.1.0.

With kind regards

This topic has been closed for replies.