STm32L496 IAP and BLE
Hi !
I've been trying to update my STM32L496 firmware over BLE.
Our bootloader use Ymodem to transfer files (as it's explained in the Application note). I have connected the UART of my BLE chip with the UART of the STM32). I can send the file (only from cygwin), and it's properly sent but my firmware is not updated. I assume that it comes from the Ymodem protocol that does not recognise the data that I transmit. I am sending the binary without Ymodem sending function, so I assume that the error comes from the fact that there is no ACK.
I can't send the binary from tera term (but from cygwin that don't have Ymodem implemented) because I use a dongle that is not recognised as a COM port.
My system will be : PC <-> dongle <-> BLE chip <-UART->STM32.
1) Is it possible to implement that Ymodem protocol in C ? from what I saw there is not so much things about this protocol.
2) Is there a better way to update my firmware ? Maybe modify my bootloader and delete Ymodem from it if it's possible ?
Thanks in advance for your help.
Florian