Skip to main content
gp73
Associate III
Jul 17, 2019 12:29 PM UTC
Solved

GCC compile and flash code

Is it possible to compile the application only with Gcc (free) so do not use GHS or Hightec and flash and run the compiled code?

I can tolerate that this compiler is not efficient as those not free.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 17, 2019 1:50 PM UTC

    Yes , it is possible for you to use gcc (free) for SPC5 Family

    The compiler is available on the update site (SPC5Studio Update site)

    http://spc5tools.spc5studio.com

    you should download from SPC5Studio Tools suite

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 17, 2019 1:50 PM UTC

    Yes , it is possible for you to use gcc (free) for SPC5 Family

    The compiler is available on the update site (SPC5Studio Update site)

    http://spc5tools.spc5studio.com

    you should download from SPC5Studio Tools suite

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.