STM32G071RB Nucleo board - Cannot write to TIM3->EGR
Cannot write to TIM3->EGR, Writes to EGR are stored in SR.
stm32g071xx.h definitions are correct.
Assembler output also shows correct addresses and offsets.
;;;1157 TIM3->DIER |= TIM_DIER_UIE;
0000b8 4608 MOV r0,r1
0000ba 68c0 LDR r0,[r0,#0xc]
0000bc 2101 MOVS r1,#1
0000be 4308 ORRS r0,r0,r1
0000c0 4922 LDR r1,|L20.332|
0000c2 60c8 STR r0,[r1,#0xc]
;;;1158 TIM3->SR |= TIM_SR_UIF;
0000c4 4608 MOV r0,r1
0000c6 6900 LDR r0,[r0,#0x10]
0000c8 2101 MOVS r1,#1
0000ca 4308 ORRS r0,r0,r1
0000cc 491f LDR r1,|L20.332|
0000ce 6108 STR r0,[r1,#0x10]
;;;1159 TIM3->EGR |= TIM_EGR_UG;
0000d0 4608 MOV r0,r1
0000d2 6940 LDR r0,[r0,#0x14]
0000d4 2101 MOVS r1,#1
0000d6 4308 ORRS r0,r0,r1
0000d8 491c LDR r1,|L20.332|
0000da 6148 STR r0,[r1,#0x14]
;;;1160 TIM3->CCMR1 |= TIM_CCMR1_CC1S;
0000dc 4608 MOV r0,r1
0000de 6980 LDR r0,[r0,#0x18]
0000e0 2103 MOVS r1,#3
0000e2 4308 ORRS r0,r0,r1
0000e4 4919 LDR r1,|L20.332|
0000e6 6188 STR r0,[r1,#0x18]
|L20.332|
DCD 0x40000400
But memory shows this.
Writes to DIER and CCMR1 are stored ok.
Writes to SR have no effect, nothing stored.
Writes to EGR are stored in SR.
0x40000400: 80 00 00 00 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00 03 00 00 00
// CR1 CR2 SMCR SR EGR CCMR1
Bug in STM32G071RB ?
Errata sheet has no matching issue...
Best regard
Juergen