Skip to main content
José Miguel Matos
Visitor II
July 16, 2019
Question

STemWin, CubeMX and L4 family

  • July 16, 2019
  • 1 reply
  • 649 views

Hi, I am trying to create a project in CubeMX for the TrueStudio but i can not connect the round LCD(MB1314). I am using the STM32L4R9I-Eval

I already tried to use the application examples present in the Repository but I only connect to an image through DSI, but with STemWin the screen never turns on.

I need help with some example or if possible with the *.ioc file.

Thanks.

This topic has been closed for replies.

1 reply

hansd56
Senior
July 23, 2019

Hi, there is an Hello World example at 'STM32 Repository\STM32Cube_FW_L4_V1.14.0\Projects\STM32L4R9I-EVAL\Applications\STemWin\MB1314\HelloWorld'. I hope this helps.