Skip to main content
Andreas Bolsch
Lead III
July 15, 2019
Question

STM32H747I-DISCO User Manual UM2411 incorrect

  • July 15, 2019
  • 1 reply
  • 602 views

The manual states two MX25QL512ABB8ESF-0SIT from

Macronix are fitted. That's wrong, there is no such device made by Macronix, in fact there are two MT25QL512ABB from Micron on the board (in accordance with the schematics).

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
July 18, 2019

Hi @Andreas Bolsch​ ,

You are right, this is an error on UM2411 and it is reported internally to be fixed.

As you said, the correct one is MT25QL512ABB8ESF-0SIT (FBGA code = RW187) from Micron.

Thanks for bringing this error to our attention.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.