Question
The interface firmware FAILED to reset/halt the target MCU FAIL.TXT message on my STEVAL-IDP005V1. How do I fix this?
I have connected STEVAL-IDP005V1 sensor board (it has an STM32F469AI ARM® Cortex®-M4 32-bit MCU on it) to the ST-LINK/V2-1 programmer/debugger on stm32 NUCLEO-F401RE board via an adapter board STEVAL-UKI001V1. When I connect the USB cable to the PC and st-link/v2-1, I see the file 'FAIL.txt' saying 'The interface firmware FAILED to reset/halt the target MCU'.
Can someone help me in fixing this? Thanks in advance
-Chandrasekhar DVS