Skip to main content
idrissmc
Associate III
July 8, 2019
Solved

Using a copy of the STM32F413H-Disco

  • July 8, 2019
  • 7 replies
  • 1392 views

Hi everyone,

I tried to copy the folder STM32Cube/cubeF4... so when i change something it doesn’t make any changes in the original folder, so then I compiled , the error was in main.c (#include “main.h�?) (no such file or directory).

thanks

This topic has been closed for replies.
Best answer by Tesla DeLorean

Should be under the project options tabs for whatever tools you are using, perhaps review docs related to "Include Paths", it is a standard C compiler concept.

0690X000009YaNKQA0.jpg

7 replies

Tesla DeLorean
Guru
July 8, 2019

So either you haven't copied all files the project consists of, or you don't have your Include Paths set up correctly.

Paths can be relative in certain tools, so a directory copy needs to maintain the same depth.

For Keil you can simple duplicate/clone a would directory, and sub-directories, at the same level

ie

...\STM32Cube\Repository\STM32Cube_FW_F4_V1.24.1\Projects\STM32F413H-Discovery\Examples\GPIO\GPIO_EXTI

to

...\STM32Cube\Repository\STM32Cube_FW_F4_V1.24.1\Projects\STM32F413H-Discovery\Examples\GPIO\GPIO_******_WINGNUT

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
idrissmc
idrissmcAuthor
Associate III
July 8, 2019

I can’t understand what you meant..

Tesla DeLorean
Guru
July 8, 2019

Which part?

The part about copying complete directories properly, and at the same level/depth?

Or the part about configuring your tools so they can search the appropriate file paths to find the files making up the project?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Cvega.11
Associate II
September 7, 2020

Hello my friend

When I connect the development board stm32h7b3i-dk to the pc through the usb to tera to use the wifi module (ISM43340-M4G-L44-10 CF), what baud rates are I have to put or what is the configuration, nothing appears in the serial communication?

Do you know how to use the wifi module (ISM43340-M4G-L44-10 CF) of the stm32h7b3i-dk board?

Any example of a WIFI http server with stm32h7b3i-dk ???