Skip to main content
garyng98
Visitor II
July 8, 2019
Question

STEVAL-BCN002V1 Sensor Demo Project Code Walk-through

  • July 8, 2019
  • 1 reply
  • 547 views

Dear all, I am new to STEVAL-BCN002V1.

I will like to inquire if there is any workshop presentation materials or materials which can explain to me the code walk-through for the entire STEVAL-BCN002V1.

As I will only use acclerometer and pressure sensor to get free-fall function, step counter, acitivites recongition.

Also, I will like to ask why am I able to add the customised C code which I had build using algobuilder to the whole project.

Please teach.

Best Regards

Gary

This topic has been closed for replies.

1 reply

Winfred LU
ST Employee
July 11, 2019

Hi Gary,

Please start from: STEVAL-BCN002V1B QUICK START GUIDE

https://www.st.com/resource/en/product_presentation/steval-bcn002v1b_quick_start_guide.pdf

Then, in after unpack the DK, there is a folder Docs with documents for your needs.

There are also user manuals or application notes available on ST web site:

https://www.st.com/en/wireless-transceivers-mcus-and-modules/bluenrg-1.html

Yes. You are able to customized firmware (C source code) for the projects.

Thank you.

Best Regards,

Winfred