Is this a documentation error? (PM0214: Cortex-M4 programming manual, NVIC base and offsets)
In section 4.3.11 NVIC register map (p.217) the base address of the main NVIC register block is stated to be 0xE000E100. The Offset to NVIC_ISER0 is then given as 0x100. This would make the address 0xE000E200.
On p. 208, however, the address of NVIC_ISER0 is given (correctly) as 0xE000E100. The other registers follow on from there.
It would therefore appear that the offsets should be corrected p.217.
However, the ARM Cortex-M4 Processor TRM gives a table of NVIC registers (section 6.2.1, p.6-63). There, there exists a register (ICTR) at offset 0x04 from 0xE000E000. So, perhaps that should be considered the base, and the offsets on p.217 would be correct...