Skip to main content
Carlos Diaz R.
Associate III
July 2, 2019
Question

Force STM32Cube MCU Package update in project.

  • July 2, 2019
  • 1 reply
  • 617 views

Hi,

I had been working with a project using a STM32F411RE device, with the STM32F4 package version 1.24.0. I installed the version 1.24.1 and would like to update the project, but when i open the Cube project it doesn't ask me for the update.

Is there any way to force the update manually?

This topic has been closed for replies.

1 reply

KnarfB
Super User
July 8, 2019

In the STM32CubeMX project manager tab, if you uncheck the "Use latest available version" you should be able to choose the correct version from the drop-down list.