Skip to main content
linusjonsson
Associate
June 21, 2019
Question

STM32L476VGT3 not booting on my pcb card

  • June 21, 2019
  • 9 replies
  • 1826 views

Hi, my mcu is not showing up in st-link v2 :(

Currently boot0 i low, 10k resistor to gnd.

All voltages are stable on vdd and no short circuit is detected.

Any tips or possible solutions to my problem?

My schematic can be found here: https://gyazo.com/836f25b0cbac1570c4dc0bceeff82472

This topic has been closed for replies.

9 replies

Tesla DeLorean
Guru
June 21, 2019

Nothing in the schematic immediately jumps out.

Pin 19 of the JTAG will have 3V from the ST-LINK on it.

What is the ST-LINK Utility or STM32 Cube Programmer reporting as a voltage on VTarget?

Check orientation of package on PCB

Check pin numbering

Check level on NRST

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
linusjonsson
Associate
June 21, 2019

Thanks for answer!

Pin 19 on jtag is nc? Should be 10k to gnd, or am I wrong here?

Nothing is showing up in ST-LINK Utility so cant see VTarget yet.

Orientation of package is ok.

What level should it be on NRST?

Tesla DeLorean
Guru
June 22, 2019

Schematic is a bit illegible, could do with being twice the resolution so the names are readable.

You have PCB image?

NRST should be high

Pin 19 is generally uncommitted, however Segger used it to output 5V and ST 3.3V, as a means to power a board. I'd leave the resistors off Pin 17 and Pin 19

ST-LINK should be able to report voltage even when it can't speak to the core.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
linusjonsson
Associate
June 22, 2019

0690X000008j4uxQAA.png0690X000008j4usQAA.png

linusjonsson
Associate
June 22, 2019

Still haven't figured out whats wrong, anyone that might know?

Piranha
Principal III
June 22, 2019

Currently boot0 i low, 10k resistor to gnd.

That is not true. R6 and R7 forms a voltage divider. Also I don't understand why do You pull R6 up to 5V, when it should normally be pulled up to VDD (3,3 V). In this case it divides voltage to 5 V / 2 = 2,5 V, which is bad, because BOOT0 pin's high level is at minimum 0,77 * 3,3 V (VDD) = 2,541 V. So it turns out to be undetermined and close to high level, but it definitely is't low level, which is at maximum 0,17 * 3,3 V (VDD) = 0,561 V. Measure the voltage on BOOT0 and at least for testing connect it to GND by switching ON switch at pin NO_1 and all other switches OFF.

Minor comment.. Reset button circuit seems to be overly complicated.

linusjonsson
Associate
June 22, 2019

Understand your point, but i have cut the trace (5V 10k) so boot0 is only connected to 10k resistor to gnd. So that should not be any problem!

Piranha
Principal III
June 22, 2019

OK, so BOOT0 is OK for now. By the way, if You didn't find it - AN4555 is pretty nice. :)

Maybe soldering problems? On LQFP packages pins can be measured with multimeter. Check all the power supply, BOOT0, NRST voltages on MCU pins. And also VSS voltages by measuring these against 3,3 V supply line.

linusjonsson
Associate
June 23, 2019

Have done some measurements, results:

VDD1: 3.29V

VDD2: 3.29V

VDD3: 3.29V

VDD4: 3.29V

VDD5: 3.29V

BOOT0: 0V

NRST: 3.17V (1.45V with ST-Link v2 unpowered) (3.17V with power)

Still nothing showing up in ST-LINK..

0690X000008j4znQAA.png