Question
Problem after jump from bootloader to RTOS application (Freertos) with call osKernelStart();
Hello,
I have problem after jump from bootloader to FreeRTOS application
I use STM32F09 (HAL) chip.
Jump from bootloader to Freertos application => OK
But when I call "osKernelStart()" board crashed
In debug I crashed in function
xPortStartScheduler()
---------------------
This is my code to jump to FreertosApplication
__entry_point = 0x0801A191
void startFirmwareApplication(void)
{
/// BOOT START APPLICATION (i.e execute SP310 FIRMWARE entry point)
MSG(" mainTask *** BOOT START APPLICATION \n");
vTaskSuspendAll();
taskDISABLE_INTERRUPTS();
__disable_irq();
__HAL_RCC_GPIOE_CLK_ENABLE();
//__HAL_RCC_GPIOB_CLK_ENABLE(); //@TODO
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Pin = GPIO_PIN_7;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_8;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
// GPIO_InitStruct.Pin = GPIO_PIN_1; //@TODO
// HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
// GPIO_InitStruct.Pin = GPIO_PIN_2;
// HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
// GPIO_InitStruct.Pin = GPIO_PIN_10;
// HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_7, GPIO_PIN_SET);
// HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_RESET); //@TODO
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_0, GPIO_PIN_SET);
// HAL_GPIO_WritePin(GPIOB, GPIO_PIN_2, GPIO_PIN_RESET); //@TODO
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_8, GPIO_PIN_SET);
// HAL_GPIO_WritePin(GPIOB, GPIO_PIN_10, GPIO_PIN_RESET); //@TODO
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
HAL_RCC_DeInit();
/* Disable all interrupts */
NVIC->ICER[0] = 0xFFFFFFFF;
/* Clear all pending interrupts */
NVIC->ICPR[0] = 0xFFFFFFFF;
/* Clear all interrupt priority */
for (int tmp = 0; tmp < 7; tmp++) {
NVIC->IP[tmp] = 0x00;
}
auto address = reinterpret_cast<uint32_t>(__entry_point);
/* change control register */
__set_CONTROL(0);
__set_MSP(address);
__entry_point();
}This is my code in Freertos appliction to remap vector table
#define FIRMWARE_START_ADDR 0x0801A191
volatile uint32_t VectorTable[48] __attribute__((section(".RAMVectorTable")));
void Remap_Table(void)
{
uint32_t i = 0;
for(i = 0; i < 48; i++)
{
VectorTable[i] = *(__IO uint32_t*)(FIRMWARE_START_ADDR + (i<<2));
}
__HAL_SYSCFG_REMAPMEMORY_SRAM();
// Enable the SYSCFG peripheral clock
__HAL_RCC_SYSCFG_CLK_ENABLE();
// Remap SRAM at 0x00000000
MX_GPIO_Init();
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port,LED_RED_Pin,GPIO_PIN_RESET);
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port,LED_BLUE_Pin,GPIO_PIN_SET);
}
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
Remap_Table();
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port,LED_RED_Pin,GPIO_PIN_SET);
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port,LED_BLUE_Pin,GPIO_PIN_RESET);
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CAN_Init();
MX_TIM16_Init();
/* USER CODE BEGIN 2 */
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port,LED_RED_Pin,GPIO_PIN_RESET);
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port,LED_BLUE_Pin,GPIO_PIN_RESET);
/* USER CODE END 2 */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* definition and creation of mainTask */
osThreadDef(mainTask, StartDefaultTask, osPriorityNormal, 0, 256);
mainTaskHandle = osThreadCreate(osThread(mainTask), NULL);
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port,LED_GREEN_Pin,GPIO_PIN_RESET);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* Start scheduler */
osKernelStart(); // board crashed here
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
can you help me please ?
Best regards
Loïc