Skip to main content
hansd56
Senior
June 19, 2019
Question

When is STM32CubeIDE going to support all STM32H7 evaluation Boards?

  • June 19, 2019
  • 0 replies
  • 509 views

I also have the STLink-V3 which I can't use with the STLink GDB in SWD mode because the only speed available is 24000KHz and fails downloading code. Using the probe with OpenOCD leaves me with no SVW support. In STM32CubeProgrammer the SWD speed is selectable???

Good to have Segger support.

When are this STM32 tools fully supported?

This topic has been closed for replies.