Skip to main content
AJouv
Associate II
June 6, 2019
Solved

[SOLVED] CAN callback never call

  • June 6, 2019
  • 4 replies
  • 1169 views

I'm working on an STM32L431 and I never be call on HAL_CAN_RxFifo0MsgPendingCallback. I have set a break point in this function but the debugger never stop on it.

In my program:

  • I have generated the code using CubeMx and I set NVIC on CAN1: Tx, RX0, RX1 and SCE
  • The cubeMx init is:
void MX_CAN1_Init(void)
{
 
 hcan1.Instance = CAN1;
 hcan1.Init.Prescaler = 5;
 hcan1.Init.Mode = CAN_MODE_NORMAL;
 hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
 hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;
 hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
 hcan1.Init.TimeTriggeredMode = DISABLE;
 hcan1.Init.AutoBusOff = ENABLE;
 hcan1.Init.AutoWakeUp = DISABLE;
 hcan1.Init.AutoRetransmission = DISABLE;
 hcan1.Init.ReceiveFifoLocked = DISABLE;
 hcan1.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan1) != HAL_OK)
 {
 Error_Handler();
 }
 
}

  • I have disable CAN filters
  • I already call HAL_CAN_ActivateNotification w/o any error returned:
(HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING)
  • Please see my CAN init:
void canDriver_init( ){
 
	// First of all enable the CAN
	HAL_GPIO_WritePin(EN_CAN_GPIO_Port, EN_CAN_Pin, GPIO_PIN_RESET);
 
	CAN_FilterTypeDef 		sFilterConfig;
 
	sFilterConfig.FilterIdHigh = 0x320 << 5;
	sFilterConfig.FilterIdLow = 0;
	sFilterConfig.FilterMaskIdHigh = 0xFFF << 5;
	sFilterConfig.FilterMaskIdLow = 0;
	sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
	sFilterConfig.FilterBank = 0;
	sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
	sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
	sFilterConfig.FilterActivation = DISABLE;
	sFilterConfig.SlaveStartFilterBank = 14;
 
	if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
	{
		/* Filter configuration Error */
		Error_Handler();
	}
 
	/* Start the CAN peripheral */
	if (HAL_CAN_Start(&hcan1) != HAL_OK)
	{
		/* Start Error */
		Error_Handler();
	}
 
	/* Activate CAN RX notification */
	if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK) {
		/* Notification Error */
		Error_Handler();
	}
 
	TxHeader.StdId = 0x320;			/* Specify the remote CAN node address			*/
	TxHeader.ExtId = 0x01;			/* Not used here								*/
	TxHeader.RTR = CAN_RTR_DATA;	/* Data Frame type (Data or Commands)			*/
	TxHeader.IDE = CAN_ID_STD;		/* Standard frame but not Extended				*/
	TxHeader.DLC = 2;				/* Number of data size in bytes (from 0 to 8)*/
	TxHeader.TransmitGlobalTime = DISABLE;
 
}

My test:

  • Send frame using my code

=> I already receive it in my CAN analyzer

  • I set a breakpoint in HAL_CAN_RxFifo0MsgPendingCallback()
  • Using a CAN analyzer I send CAN frame

=> but those frame never be received by the STM32 (I already see the hardware signal on the medium using an oscilloscope)

Thanks for your help

Regards

This topic has been closed for replies.
Best answer by AJouv

I slove the issue by activate the filtre:

	CAN_FilterTypeDef 		sFilterConfig;
	sFilterConfig.FilterIdHigh = 0x0000;
	sFilterConfig.FilterIdLow = 0x0000;
	sFilterConfig.FilterMaskIdHigh = 0x0000;
	sFilterConfig.FilterMaskIdLow = 0x0000;
	sFilterConfig.FilterFIFOAssignment = 0;
	sFilterConfig.FilterBank = 0;
	sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
	sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
	sFilterConfig.FilterActivation = ENABLE;
	sFilterConfig.SlaveStartFilterBank = 14;

If the FilterActivation is not ENABLE it was impossible to receive CAN frame.

4 replies

Glen Cook_2
Associate II
June 7, 2019

The code looks fine. I would first try fully opening the can filter to let everything through, see if anything triggers the interrupt.

AJouv
AJouvAuthor
Associate II
June 7, 2019

Hello @Community member​ ,

First of all, Thanks for your help.

In my understanding, the filter is already disable and not used in my config because I have set:

sFilterConfig.FilterActivation = DISABLE;

is it true ?

AJouv
AJouvAuthor
Associate II
June 13, 2019

Anyone have an idea to help me ?

Thanks

AJouv
AJouvAuthorBest answer
Associate II
June 25, 2019

I slove the issue by activate the filtre:

	CAN_FilterTypeDef 		sFilterConfig;
	sFilterConfig.FilterIdHigh = 0x0000;
	sFilterConfig.FilterIdLow = 0x0000;
	sFilterConfig.FilterMaskIdHigh = 0x0000;
	sFilterConfig.FilterMaskIdLow = 0x0000;
	sFilterConfig.FilterFIFOAssignment = 0;
	sFilterConfig.FilterBank = 0;
	sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
	sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
	sFilterConfig.FilterActivation = ENABLE;
	sFilterConfig.SlaveStartFilterBank = 14;

If the FilterActivation is not ENABLE it was impossible to receive CAN frame.