Skip to main content
Central SUPPORT
Senior
June 4, 2019
Solved

How to disable L6599 output

  • June 4, 2019
  • 1 reply
  • 1244 views

I am using an L6599A high voltage resonant controller in my AC/DC power supply, and I want to add a shutdown feature. I have pulled the STBY pin to GND of the chip, however the output continues to produce pulses.

Latching shutdown (via DIS pin) is not what I want, so is there any other way to stop output pulses without removing AC power from my system?

 

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This topic has been closed for replies.
Best answer by Central SUPPORT

There are two ways how to achieve the desired function:

1.    The VCC pin can be pulled below VCC_OFF threshold (7.45V). See Table 5 “Electrical Characteristics�? of datasheet for more information.

2.    The LINE pin can be pulled below 1.24V. See chapter 7.6 “Line sensing function�? of datasheet for more information.

1 reply

Central SUPPORT
Central SUPPORTAuthorBest answer
Senior
June 4, 2019

There are two ways how to achieve the desired function:

1.    The VCC pin can be pulled below VCC_OFF threshold (7.45V). See Table 5 “Electrical Characteristics�? of datasheet for more information.

2.    The LINE pin can be pulled below 1.24V. See chapter 7.6 “Line sensing function�? of datasheet for more information.