Question
I do not know what version of CubeMx this project was made with. (eg Version 5.1.0) I also do not know what version of the firmware package it is.(eg STM32Cube FW_F1 V1.3.1)
I downloaded the project (using CubeMx) from GITHUB, which was already made.
But I do not know what version of CubeMx this project was made with. (eg Version 5.1.0)
I also do not know what version of the firmware package it is.
(eg STM32Cube FW_F1 V1.3.1)
This project is a project made four months ago.
Is there anyone who can answer these two questions?
Currently, I am using the latest version of CubeMx.
Thank you. ^^