Skip to main content
Rajkiran
Visitor II
May 27, 2019 9:44 AM UTC
Question

Is there any example program for HAL_FLASHEx_ComputeCRC function

Hi,

I wish to know is there any example program for calculating CRC for flash Bank using "HAL_FLASHEx_ComputeCRC() " HAL driver.

This topic has been closed for replies.

9 replies

SF??r
Associate III
Jun 7, 2019 9:28 AM UTC

Hello,

would be interessing for me as well... on a broken Y revision I give up at the moment...

My source to check an erased (0xFF) second flash bank looks like this:

	 FLASH_CRCInitTypeDef crchandle = { 0 };
	 crchandle.Bank = FLASH_BANK_2;
	 crchandle.CRCStartAddr = FLASH_BANK2_BASE;
	 crchandle.CRCEndAddr = FLASH_BANK2_BASE + 0x100;
	 crchandle.TypeCRC = FLASH_CRC_ADDR;
	 crchandle.BurstSize = FLASH_CRC_BURST_SIZE_4;
 
	 uint32_t crc_out = 0;
	 HAL_FLASHEx_Unlock_Bank2();
	 FLASH->CRCCR2 = 0; //workaround
	 if(HAL_OK == HAL_FLASHEx_ComputeCRC(&crchandle, &crc_out))
		 logging_debug(LOGMOD_USBHOST, "CRC blocking: 0x%08X", crc_out);
	 HAL_FLASHEx_Lock_Bank2();

But fails...

Why? Errate says: Do not use Flash CRC but also that just fails at sector 7 ?!?!?!?!?!?!

Tesla DeLorean
Guru
Jun 7, 2019 12:51 PM UTC

Code fragment works on the V step

Core=400000000, 400 MHz

CPUID 411FC271 DEVID 450 REVID 2003

Cortex M7 r1p1

STM32H7xx

CRC blocking: 0x349A943E

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SF??r
Associate III
Jun 7, 2019 1:42 PM UTC

Hm, did you check the crc output?

I didn't get this result if I check it with this website:

http://www.sunshine2k.de/coding/javascript/crc/crc_js.html

Here the 256 Bytes flash data:

0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF

Tesla DeLorean
Guru
Jun 7, 2019 3:53 PM UTC

>>Hm, did you check the crc output?

I didn't, but it is not blank, it has code for the CM4 core in it. I thought the issue was it seized up. Will cross-check the data later.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SF??r
Associate III
Jun 17, 2019 5:41 AM UTC

Have a V Revision now....

Same test: 0xB02CC19B

makes even no sense?! Can anyone help?

Tesla DeLorean
Guru
Mar 5, 2020 9:16 PM UTC

The minimum size seems to be 512-bytes (at burst 4).

I can make the sector (128KB), and bank (1MB) generate the same numbers as the equivalent address span.

So the numbers are consistent, but the math is not, currently got a query in about that.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Mar 5, 2020 10:45 PM UTC
void flash_crc_test(void)
{
 FLASH_CRCInitTypeDef CRCInit = {};
 HAL_StatusTypeDef st;
 uint32_t CRC_Result;
 
 ttyprintf("Enter sector num. to CRC (0-15), or B1/B2 for whole bank:");
 char *s = tty_getline();
 if (!s) goto error;
 if (s[0] == 'b' || s[0] == 'B') {
 // CRC on bank
 CRCInit.TypeCRC = FLASH_CRC_BANK;
 if (s[1] == '1') {
 CRCInit.Bank = FLASH_BANK_1;
 } else if (s[1] == '2') {
 CRCInit.Bank = FLASH_BANK_2;
 }
 else {
 goto error;
 }
 } else {
 // CRC on sector
 CRCInit.TypeCRC = FLASH_CRC_SECTORS;
 CRCInit.Sector = atoi(s);
 CRCInit.Bank = FLASH_BANK_1;
 if (CRCInit.Sector >= FLASH_NUM_SECTORS_PER_BANK) {
 CRCInit.Bank = FLASH_BANK_2;
 CRCInit.Sector -= FLASH_NUM_SECTORS_PER_BANK;
 }
 CRCInit.NbSectors = 1;
 }
 CRCInit.BurstSize = FLASH_CRC_BURST_SIZE_256;
 CRCInit.CRCEndAddr = 0;
 CRCInit.CRCStartAddr = 0;
 
 // Unlock:
 if (CRCInit.Bank == FLASH_BANK_1) {
 st = HAL_FLASHEx_Unlock_Bank1();
 } else {
 st = HAL_FLASHEx_Unlock_Bank2();
 }
 if (st != HAL_OK) {
 ttyprintf("Flash unlock failed!\n");
 goto error;
 }
 
 uint32_t start_time = HAL_GetTick();
 st = HAL_FLASHEx_ComputeCRC(&CRCInit, &CRC_Result);
 if (st == HAL_OK) {
 ttyprintf("CRC=%8.8X time=%u ms\n", (unsigned)CRC_Result, (unsigned)(HAL_GetTick() - start_time));
 } else {
 ttyprintf("CRC calc error!\n");
 }
 return;
 error:
 ttyprintf("Error\n");
}

This example is for STM32H743/753 with two banks, 8 blocks each.

Don't forget to unlock.

-- pa

BTrav.1
Visitor II
Nov 14, 2020 2:05 AM UTC

Same issue for me - I'm running the FLASH CRC across an erased section of FLASH, aligned to my burst size, and I get 0xb02cc19b - same value you got. I went through the datasheet with a fine-tooth comb and stepped through the code, watching registers, and everything looks right, but it's giving the wrong results. (This is a STM32H753, silicon V) I'm starting to wonder if there's something missing like an erased value doesn't read 0xFF to the CRC module or there's another clock enable I need or something...

Did you ever get it figured out?

Associate II
Nov 14, 2024 4:22 PM UTC

Hello,

Any news on the topic ? I observe same issue