Skip to main content
SJabl
Visitor II
May 24, 2019
Question

SPC5-UDESTK Tool

Hello,

Im searching for a simple solution to flash several prototypes.

Since our Lauterbach Debugger has been used for HIL testing there is the need for

a 2nd solution.

Recently there are two Questions left:

1. Is it possible to flash also NXP/Freescale 5604 types using the SPC5-UDESTK oder is this locked ? (We have mixed Yield depending on the REV of the PCB)

2. Can I use Trace32 from Lauterbach with the SPC5-UDESTK ?

thx in advance.

    This topic has been closed for replies.

    1 reply

    Matthias Noack
    Visitor II
    June 27, 2019

    SPC5-UDESTK is usable with STM controllers only.

    For a stand alone flash solution with automation capabilities have a look at PLS's website www.pls-mc.com