Larger HID report greater than 8 bytes
I am running interrupt data transfer in HS mode (with ULPI chip, and can do see interrupts at the HS rate of 8kHz). So I can get an HID report of 8 bytes, but I can get above that. I set the USB end point descriptor to 16 was 8. I added one byte to my report by incrementing a report count for an 8 bit field. And changed USBD_HID_SendReport to send 9 bytes. This worked as I slowly went from 4 bytes in the mouse example to 8 bytes, but I can't get above that.
For those familiar with BusHound it is reporting babble detected when a report should be sent back.
Thanks in advance