Skip to main content
G.M.
Associate
May 22, 2019
Question

CANNOT FIND "Connect Under Reset" option in the Target -> settings menu in the STM32 ST_LINK utility. The primary problem is that i cannot connect my st_link to the utility. I have aready updated the firmware

..

    This topic has been closed for replies.

    6 replies

    waclawek.jan
    Super User
    May 22, 2019

    Target->Settings, a Settings window opens:

    0690X000008wGj4QAE.png

    JW

    G.M.
    G.M.Author
    Associate
    May 22, 2019

    I haven't that option on the list, i only have Normal and Hot Plug options

    G.M.
    G.M.Author
    Associate
    May 22, 2019

    And i also can't modify the frequency in the port configuration section

    Tesla DeLorean
    Guru
    May 22, 2019

    Not much to work with here. Doesn't find the ST-LINK? Doesn't find the Target the ST-LINK is attaching too?

    What version of the Utility? What board or ST-LINK pod involved.

    0690X000008wGjJQAU.jpg

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    G.M.
    G.M.Author
    Associate
    May 22, 2019

    It find ST-LINK, version V1, i am using an stm8s discovery demoboard

    waclawek.jan
    Super User
    May 22, 2019

    Ah, V1 has its limitations...

    But you should be able to do "connect under reset" also "manually" - hold the NRST line low, while attempting to connect. If it does not work, you have a serious problem.

    Is the original target (the STM8) disconnected? Do you use a short cable to connect to the STM32 target?

    JW