Skip to main content
NKupe
Associate II
May 22, 2019
Solved

Error: E31 Remote Failure Reply, when starting code in debug mode

  • May 22, 2019
  • 5 replies
  • 8642 views

Hello all, I am currently trying to get my STM32F411RE code working in Atollic TrueStudio. This project leverages the use of DMA and CMSIS-DSP which are all working in TrueStudio to find freqeuncy outcomes. The issues at hand is that I can upload my code to the STM32 board in the debug mode, but that this crashes once I attempt to resume the code and execute the main loop.

I upload the code to the board using the ST32 Cubeprogrammer CLI, which downloads and verifies the code without any hiccups. It then switches over to the ST-Link which executes the setup code and stops at the (auto inserted per GDB) breakpoint just before the main. Executing the code then yields:

TraceCaptureStart and SWV event set to APP_TRUE
ST-LINK device status: RUN_MODE
 
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying....
 
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying....
 
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying....

It then keeps repeating those 2 lines until it times out and kicks me back to the editor environment.

Then by using the GDB Trace option (inside the debug configurations) I was able to find that the resulting error is

Warning: remote failure reply: E31

which by searching around (on this forum) yielded that this is an error with the GDB server. I tried to run the GDB server as a remote client, but this yielded the exact same issues. This link shows the GDB trace code up until the breakpoint (https://pastebin.com/9kygHtwD), whilst this link shows the code after proceeding past the breakpoint by resuming the code execution (https://pastebin.com/tHNwR7Hy).

I am now wondering if perhaps it has something to do with the code itself? I have included my total code here (https://pastebin.com/XWsS7urd), whilst the setup() and main() can be found here (https://pastebin.com/Lj24zvge).

Because of these errors I also have to erase my chip (ST-Link or STCubeProgrammer) after debugging before I can upload my code again; I presume this is because of the board not being shutdown correctly with the debugger crashing? Or would I need to do this always?

EDIT: as per my reaction in the comments, I have tried to upload a newly generated project (from CubeMX) onto the board and I still get the same issues. So it is either something to do with my toolchain or it is due to the STCubeMX standard code

This topic has been closed for replies.
Best answer by Tesla DeLorean

Low power modes where debug interface is turned off. ie WFI

Reconfiguring of pins used by the debug interface.

Debugger breaking real-time deadlines for interrupt/peripheral service.

DMA operations which continue which CPU stalled in debugger waiting for human interaction.

Check connect under reset options, or BOOT0=HIGH settings, if your code blocks debugger connection/programming.

5 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 22, 2019

Low power modes where debug interface is turned off. ie WFI

Reconfiguring of pins used by the debug interface.

Debugger breaking real-time deadlines for interrupt/peripheral service.

DMA operations which continue which CPU stalled in debugger waiting for human interaction.

Check connect under reset options, or BOOT0=HIGH settings, if your code blocks debugger connection/programming.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
NKupe
NKupeAuthor
Associate II
May 22, 2019

As for the low power modes, I have not intentionally set up any of them in the user code, but perhaps such a mode is instigated by the code generated by CubeMX when the chip is idling?

Regarding the reconfiguring of pins, I use the USB micro B connector on the board with ST-Link for debugging. So I dont think it is possible to change the pins?

EDIT: I have since tried to flash a completely empty project on to the board, using only code that was generated by the STCubeMX. I still get the same errors, so either it is due to boiler plate code that STCubeMX produces or it has got something to do with the ST-Link / STCubeProgrammer itself

NKupe
NKupeAuthor
Associate II
May 22, 2019

I have since figured out that the issues lies with the startup scripts in the debug configuration. The Target Software Startup Scripts I had for my debug that caused the crashing is:

# Set flash parallelism mode to 32, 16, or 8 bit when using STM32 F2/F4 microcontrollers
# Uncomment next line, 2=32 bit, 1=16 bit and 0=8 bit parallelism mode
#monitor flash set_parallelism_mode 2
 
# Set character encoding
set host-charset CP1252
set target-charset CP1252
 
# Reset to known state
monitor reset
 
# Load the program executable
load		
 
# Reset the chip to get to a known state. Remove "monitor reset" command 
# if the code is not located at default address and does not run by reset. 
monitor reset
 
# Enable Debug connection in low power modes (DBGMCU->CR)
set *0xE0042004 = (*0xE0042004) | 0x7
 
# Set a breakpoint at main().
tbreak main
 
# Run to the breakpoint.
continue

Whilst the code that lets me run the main loop in the debugger is:

# Set flash parallelism mode to 32, 16, or 8 bit when using STM32 F2F4 microcontrollers
# 2=32 bit, 1=16 bit and 0=8 bit parallelism mode
monitor flash set_parallelism_mode 2
 
# Load the program executable
load		
 
# Enable Debug connection in low power modes (DBGMCU-CR)
set 0xE0042004 = (0xE0042004) 0x7
# Set a breakpoint at main().
tbreak main
 
# Run to the breakpoint.
continue

I am not sure yet what is faulty about the first code, but I will evaluate it and post my findings

NChor.1
Associate II
July 3, 2022

Put a jumper on your ST Link V2(VDD(19) and TVCC(1))