Skip to main content
MKubi
Visitor II
May 22, 2019
Question

Interrupt RX isn't called on STM32F413ZH Nucleo board

  • May 22, 2019
  • 0 replies
  • 484 views

What is wrong with the following code that the RX Interrupt isn't called. On the osziloscope I see Send and Receive correctly.

HAL_Init();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_USART6_CLK_ENABLE();

#define CONSOLE_TXD_PIN LL_GPIO_PIN_11

/* Configure Tx Pin as : Alternate function, High Speed, Push pull, Pull up */

LL_GPIO_SetPinSpeed(GPIOA, CONSOLE_TXD_PIN, LL_GPIO_SPEED_FREQ_HIGH);

LL_GPIO_SetPinOutputType(GPIOA, CONSOLE_TXD_PIN, LL_GPIO_PULL_NO);

LL_GPIO_SetPinPull(GPIOA, CONSOLE_TXD_PIN, LL_GPIO_PULL_UP);

LL_GPIO_SetPinMode(GPIOA, CONSOLE_TXD_PIN, LL_GPIO_MODE_ALTERNATE);

LL_GPIO_SetAFPin_8_15(GPIOA, CONSOLE_TXD_PIN, LL_GPIO_AF_8);

#define CONSOLE_RXD_PIN LL_GPIO_PIN_12

/* Configure Rx Pin as : Alternate function, High Speed, Push pull, Pull up */

LL_GPIO_SetPinSpeed(GPIOA, CONSOLE_RXD_PIN, LL_GPIO_SPEED_FREQ_HIGH);

LL_GPIO_SetPinOutputType(GPIOA, CONSOLE_RXD_PIN, LL_GPIO_OUTPUT_PUSHPULL);

LL_GPIO_SetPinPull(GPIOA, CONSOLE_RXD_PIN, LL_GPIO_PULL_UP);

LL_GPIO_SetPinMode(GPIOA, CONSOLE_RXD_PIN, LL_GPIO_MODE_ALTERNATE);

LL_GPIO_SetAFPin_8_15(GPIOA, CONSOLE_RXD_PIN, LL_GPIO_AF_8);

NVIC_SetPriority(USART6_IRQn, 0);

NVIC_EnableIRQ(USART6_IRQn);

LL_USART_EnableIT_TXE(USART6);

LL_USART_EnableIT_RXNE(USART6);

LL_USART_SetTransferDirection(USART6, LL_USART_DIRECTION_TX_RX);

/* 8 data bit, 1 start bit, 1 stop bit, no parity */

LL_USART_ConfigCharacter(USART6, LL_USART_DATAWIDTH_8B, LL_USART_PARITY_NONE, LL_USART_STOPBITS_1);

LL_USART_SetHWFlowCtrl(USART6, LL_USART_HWCONTROL_NONE);

/* Reset value is LL_USART_OVERSAMPLING_16 */

LL_USART_SetOverSampling(USART6, LL_USART_OVERSAMPLING_16);

const uint32_t pclk = __LL_RCC_CALC_PCLK2_FREQ(SystemCoreClock,

LL_RCC_GetAPB2Prescaler());

LL_USART_SetBaudRate(USART6, pclk, LL_USART_OVERSAMPLING_16, 9600);

LL_USART_Enable(USART6);

This topic has been closed for replies.