Skip to main content
Bnaga
Associate
May 21, 2019
Question

HI , i wanted Interface STM32F401RE nucleo To SDIO_4_ bit+Fatfs , SD card Can anyone help me to construct the Hardware Circuit.for this??????

  • May 21, 2019
  • 2 replies
  • 1409 views

..

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 21, 2019

https://www.waveshare.com/micro-sd-storage-board.htm or equivalent

The SDIO pins are at the north end of the two connectors

PC8 D0

PC9 D1

PC10 D2

PC11 D3

PC12 CLK

PD2 CMD

3V

GND

33K or 47K pull-ups on Dx and CMD pins (socket above has these, bare sockets won't)

Could use one of the other near GPIO for card detect.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Bnaga
BnagaAuthor
Associate
May 21, 2019

Hi sir,

I used 4.7k , 20 k , 47 k, with using an jumper wires connections with stm32f401re nucleo board, but i am not able to find the SD CARD MOUNT IN PC .......

I GENERATED THE CODE AS PER ST CUBE MX..

I USED SDIO+FATFS MW FOR MY PROJECT..

GUIDE ME TO DO FURTHER I WILL REFER YOUR REFRENCES ALSO .

THANK YOU FOR SUPPORTS