Skip to main content
Steve Fairhead
Associate II
May 19, 2019
Question

STM32F767VIT6: SAI1 USB issue

  • May 19, 2019
  • 0 replies
  • 506 views

I'm working on a board where SAI1 is wired to a DAC. I've had it working using HAL calls, from a wavetable in RAM. But it needs to play back audio from USB. I tried various approaches; no luck. I was pointed at:

STM32Cube_FW_F7_V1.15.0\Projects\STM32746G-Discovery\Applications\USB_Device\AUDIO_Standalone

This uses SAI2. I have this dev board; I compiled it and ran it; it wasn't perfect (some scratchiness), but was close enough. But it uses the SAI Driver, not the HAL calls.

I ported it to my board, changing only SAI2 to SAI1 (and the CPU); doesn't work. Tried various other approaches, same result. No output - no clocks, nothing - from the SAI1 block.

Under debug, watching the registers, I see SAI1 B registers being setup. I need SAI1 A. Is there a bug in the driver? If not, what am I missing?

I could, I guess, re-use my original HAL-based code - but the USB interface code is more complex than I have time to analyse.

Steve

This topic has been closed for replies.