Skip to main content
Raghu
Associate
May 17, 2019
Solved

How to fix the power consumption of STC3115?

  • May 17, 2019
  • 1 reply
  • 1406 views

I have a design with STC3115AIQT as in picture:

0690X000008w2F0QAI.jpg

VBAT and GND are connected to positive and negative terminals of a Li-Ion battery, respectively.

When the device is powered-off 3V_L is connected to GND. In this condition VIN pin is sinking 3mA of current, i.e. Voltage across R15 is 3V.

Why is it so abnormally high compared to the value stated in datasheet (1µA)? How can I fix it?

This topic has been closed for replies.
Best answer by LHugh

0690X00000AQSkTQAX.jpgThe datasheet shows the VCC pin connected to the battery so it is not powered down while VBAT is connected to VIN.

I suspect the device is not designed to work like that and is effectively shorting VIN to ground while it is not powered up via VCC.

I think you need to keep the STC3115 powered by the battery whle the rest of the system powers down.

1 reply

LHugh
LHughBest answer
Visitor II
September 3, 2019

0690X00000AQSkTQAX.jpgThe datasheet shows the VCC pin connected to the battery so it is not powered down while VBAT is connected to VIN.

I suspect the device is not designed to work like that and is effectively shorting VIN to ground while it is not powered up via VCC.

I think you need to keep the STC3115 powered by the battery whle the rest of the system powers down.