ggyy426Associate IIIForum|Forum|7 years agoMay 16, 2019QuestionTouchGFX taget MDK-ARM debug fault (Automatic run without clicking run )Forum|Forum|7 years agoMay 16, 201913 replies4941 viewsHi allI try to use MDK-ARM Keil to debug TouchGFX project?But it hang on Debug mode.When enter debug it directly run and hang like photo belowThis happen after I add new algorithm for STM32H7 After adding this for QSPI setting for insufficient flashBecause I code and photo are more than 2MBs so I need add .flm file to use QSPIHere is my fileThanksDemo.rarQSPISTM32H7 seriesTouchGFXKeil