Input Cupture values sometime skipped on DMA Circular mode
My environment is Nucleo-F446RE(STM32F446) with TrueSTUDIO / CubeMX on Windows 10.
I tried to get a 6MHz frequency signal by Input Capture module. However, modules often skip timer values.



/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint16_t captures[240];
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_3) {
}
}
void HAL_TIM_IC_CaptureHalfCpltCallback(TIM_HandleTypeDef *htim)
{
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_3) {
}
}
/* USER CODE END 0 */
int main(void)
{
/* USER CODE BEGIN 2 */
HAL_TIM_IC_Start_DMA(&htim2, TIM_CHANNEL_3, captures, 120);
/* USER CODE END 2 */
}
This is an example of an aquired buffer(captures[240]) on my environment.
[825, 840, 856, 864, 2653, 2668, 2684, 2700, 4465, 4481, 4497...]
Interval between signals are should always from 10 to 20, but it has more than 2000.
This problem doesn't occur when I change DMA mode from "Circular" to "Normal". But I'm concerned about processor efficiency because a frequency of this signal is very high,
Can I avoid this trouble about Input Capture with DMA Circular mode by modifying the program?