STM32H7 and u-SD card on sdmmc1 - Using STM32CubeMX and HAL
- May 9, 2019
- 10 replies
- 5910 views
Dear friends,
I'm Using STM32Cube_FW_H7_V1.4.0 with TrueStudio 9.3.0, on an STM32H753.
Has anybody got an micro-SD card working on the SDMMC1 peripheral for an STM32H7?
For my it, seems to come with a Timeout error.
I initialized it like:
void MX_SDMMC1_SD_Init(void)
{
HAL_StatusTypeDef status;
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 2; // 0 - 1023
status = HAL_SD_Init(&hsd1);
if (status != HAL_OK)
{
dmc_puts("!HAL_OK\n");
_Error_Handler2(__FILE__, __LINE__, status);
// Error_Handler();
}
}
void HAL_SD_MspInit(SD_HandleTypeDef* sdHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(sdHandle->Instance==SDMMC1)
{
/* USER CODE BEGIN SDMMC1_MspInit 0 */
/* USER CODE END SDMMC1_MspInit 0 */
/* SDMMC1 clock enable */
__HAL_RCC_SDMMC1_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**SDMMC1 GPIO Configuration
PC8 ------> SDMMC1_D0
PC9 ------> SDMMC1_D1
PC10 ------> SDMMC1_D2
PC11 ------> SDMMC1_D3
PC12 ------> SDMMC1_CK
PD2 ------> SDMMC1_CMD
*/
GPIO_InitStruct.Pin = SD_D0_Pin|SD_D1_Pin|SD_D2_Pin|SD_D3_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDIO1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = SD_CK_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDIO1;
HAL_GPIO_Init(SD_CK_GPIO_Port, &GPIO_InitStruct); // GPIOC
GPIO_InitStruct.Pin = SD_CMD_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDIO1;
HAL_GPIO_Init(SD_CMD_GPIO_Port, &GPIO_InitStruct); // GPIOD
/* SDMMC1 interrupt Init */
HAL_NVIC_SetPriority(SDMMC1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SDMMC1_IRQn);
/* USER CODE BEGIN SDMMC1_MspInit 1 */
/* USER CODE END SDMMC1_MspInit 1 */
}
}The call MX_SDMMC1_SD_Init(); was missing the lines to call HAL_SD_Init(&hsd1);, which I added.
I printed some messages, which I added to the HAL Libraries:
MX_SDMMC1_SD_Init
SDMMC_ERROR_TIMEOUT
ERROR: SD_PowerON
ERROR: HAL_SD_InitCard
!HAL_OK
Besides 4-bit mode, I tried 1-bit mode, and I experimented with the clock speed.
And I tried different SD Cards, all with the same result.
What can I check?
My source code is also on github, I will comment back and update it once it works, so it can help others.
https://github.com/bkht/STM32_SD_SDMMC
I have used an eMMC on SDMMC (8-bit) on an STM32F7, but this SD Card (4-bit) is on an STM32H7.