Skip to main content
MikeDB
Senior II
May 9, 2019
Solved

Is it possible to mute a particular warning in the STM32CubeIDE compiler ?

  • May 9, 2019
  • 3 replies
  • 3746 views

I had to create some register variables and inline assembler to enforce use of the M7's SMLAL instruction and now keep getting the warning several times per compile :

warning: optimization may eliminate reads and/or writes to register variables [-Wvolatile-register-var]

Is it possible to mute just this particular warning ? I went to the Files->Properties->Warnings page and there are various tickboxes but I can't see a way to mute a particular warning.

This topic has been closed for replies.
Best answer by After Forever

Is there a place in the Settings to add a custom compiler option? Just adding "-Wno-volatile-register-var" there should do the work.

Or, you could temporarily disable the warning only for those lines you want:

#pragma GCC diagnostic push
#pragma GCC diagnostic ignored "-Wvolatile-register-var"
/* code generating the warning */
#pragma GCC diagnostic pop

3 replies

After Forever
After ForeverBest answer
Senior III
May 9, 2019

Is there a place in the Settings to add a custom compiler option? Just adding "-Wno-volatile-register-var" there should do the work.

Or, you could temporarily disable the warning only for those lines you want:

#pragma GCC diagnostic push
#pragma GCC diagnostic ignored "-Wvolatile-register-var"
/* code generating the warning */
#pragma GCC diagnostic pop

MikeDB
MikeDBAuthor
Senior II
May 9, 2019

Thanks - I hadn't thought of using a pragma. I can see the real warnings now.

MikeDB
MikeDBAuthor
Senior II
May 9, 2019

It seems to just be tickboxes. The only field that looks where it looks like it should go is in the Settings->GCC Compiler->Tool Settings but this field is greyed out and so not editable, presumably to stop people making silly mistakes.