Skip to main content
SAhme.0
Visitor II
May 8, 2019
Question

Why motor profiler is not running with STM3240G-Eval with STEVAL-IHM028V2?

  • May 8, 2019
  • 1 reply
  • 625 views

We have STM3240G-Eval and STEVAL-IHM028V2 boards.

we are trying to run the bldc motor of (24 pole-pairs,1.4KW) with motor profiler (MC-SDK 5.3.3) and we also tried with another motor (8 pole-pairs , 30W) .

the profiler isn't able to calculate Rs, Ls and Ke Values. but after 20% to 25% of profiling it is showing "The measurement is talking too much time".

we also decrease current and max. speed but the result are same.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards