sagarAssociate IIForum|Forum|7 years agoMay 7, 2019QuestionWhat should be the output value of ADC if input is not connected to dedicated pin? I am getting some values (230).Forum|Forum|7 years agoMay 7, 20192 replies1287 viewsHello, As I am working on analog inputs I require ADC. STM32F334 Nucleo board has 12-bit ADC (2) with 21 channels, I am using ADC1 Channel 1.After programming without applying any input to the pin (PA0) I am getting some values through USART2.Can anybody help me out.Thanks in advance.STM32F3 seriesADC