Associate III
May 7, 2019
Question
Setting CubeMX Files as Reference not generated project files
- May 7, 2019
- 5 replies
- 3260 views
When Creating STM32Cube Project ,
While Selecting Code Generation Option as "Add necessary library files as reference in the toolchain project configuration file"
Then giving Finish will result the following
"Code Generation could not be done because the necessary firmware package is missing
Not able to complete STM32Cube project creation"
I am using
STM32CubeIDE V1.0
STM32Cube_FW_F4 1.24.1
Kindly rectify this