Skip to main content
SSchm.5
Associate III
May 5, 2019
Question

JTAG lost after SystemClock_Config

  • May 5, 2019
  • 8 replies
  • 1469 views

Hello,

I'm currently working of a project based on a CubeMX generated code.

I'm currently experiencing something strange.

I use a Segger J-link as a programming interface. When I want to debug my program, as I can see, the program arrive inside "SystemClock_Config" function. I check that everything is ok with breakpoints and it don't seem to create error.

But after finishing this function the JTAG connection is lost like the board is disconnected.

I reproduced the problem at least 10 times to be sure it was not due to a bad contact on my board.

I would like to know if is some clock configurations can create this kind of problem.

Thank you,

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
May 5, 2019

Specific STM32?

Reprogramming GPIOA bank can be an issue, there might also be some settings to disable SWD/JTAG depending on how you configured CubeMX

Going into low power modes can also turn off the chip so the scan chains are not functional.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SSchm.5
SSchm.5Author
Associate III
May 5, 2019

Yes, specific STM32.

What kind of low power features in CubeMX could cause that?

I double checked that JTAG was properly set in the configuration (JTAG 4 pins) and the GPIOA don't seem to have time to be modified at this time.

Thank you for your answer.

Tesla DeLorean
Guru
May 5, 2019

What specific STM32 part, there's like a dozen families, and a hundred parts these days...

Not a CubeMX user, but remember a Debugger setting.

So bisect the executing code in SystemClock_Config() to pin down which section causes the failure, can't see what it's doing from here.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SSchm.5
SSchm.5Author
Associate III
May 6, 2019

My bad. I understood your question as if I experienced this problem only with ST's MCU. Fatigue is the worst enemy.

It's a STM32F446RE.

I tried to debug the SystemClock_Config() function but nothing seemed wrong. I will try again.

Amel NASRI
ST Technical Moderator
May 8, 2019

Hi @Community member​ ,

Please note that there is a limitation in STM32F4 devices where you cannot use Full JTAG configuration without NJTRST pin.

This is explained in errata sheet file.

So, JTAG 4 pins cannot be used and shouldn't be allowed from STM32CubeMX.

This will be reported to our STM32CubeMX experts.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
SSchm.5
SSchm.5Author
Associate III
May 13, 2019

I checked in CubeMX and changing JTAG 4 pins to serial wire don't force me to use some unconnected pins of my design. So I think I will be able to use my J-Link with a ST-Link configuration in Atollic. Or worst case, I will have to wire the connector to my ST-link so it's just minimal pain.

Thank you,

SSchm.5
SSchm.5Author
Associate III
May 21, 2019

Hello,

I'm back here due to the same kind of problem...

I've assembled my design with a new board (I corrected some mistakes which don't imply the uC) and now, the J-link can't even find the uC.

Here is the design:

0690X000008wA61QAE.jpg

and here is the board:

0690X000008wA6kQAE.jpg

What you see highlighted is the LDO 3.1V line from an STNS.

What I checked on my board with an oscilloscope is that JTDO is the only signal which don't seem to be properly driven. The signal is very noisy and I can perceive that it try to answer but the noisy signal just have a slightly higher average.

I tried to connect the Needle 10 pins to an ST-link and it don't work either.

If you have an idea...

Thank you.

Piranha
Principal III
May 21, 2019

Well, You should read AN4488...

  • VDDA is unpowered... And no - it's not only for ADC and DAC, but also internal RCs, PLLs, reset circuit and possibly something else.
  • VCAP1 is wrong. It must be 4,7 uF and I suggest it to be at least 10V X7R 1206.
  • VDD capacitors also doesn't follow recommendation - these should be 4,7 uF + 4 * 100 nF. I suggest 4,7 uF to be at least 10V X5R 0805.
  • That long two part supply route is bad. Make a single branch for MCU and put recommended VDD capacitors to it.