Skip to main content
andreaspiezia9
Associate III
May 4, 2019
Solved

HAL_UART_Transmit doesn't work

  • May 4, 2019
  • 2 replies
  • 1667 views

Hi,

I'm simply want transmit on UART using code generated by CUBEMX 5.1.0 for NUCLEO F401RE in System Workbench (Version: Neon.3 Release (4.6.3)).

I've only added the following code in the main:

UartStatus is ALWAY HAL_OK after every transmission. I'm using Tera Term to see the serial data on COM5.

Thanks for help!

0690X000008BH2TQAW.png

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 uint8_t buffer [] = {0,1,2,3};
 UartStatus = HAL_UART_Transmit(&huart2, buffer, 4, 1000);
 if (UartStatus != HAL_OK)
 {
	 HAL_Delay(1000);
 }
 
 HAL_Delay(1000);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
 
static void MX_USART2_UART_Init(void)
{
 
 /* USER CODE BEGIN USART2_Init 0 */
 
 /* USER CODE END USART2_Init 0 */
 
 /* USER CODE BEGIN USART2_Init 1 */
 
 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */
 
 /* USER CODE END USART2_Init 2 */
 
}
 

This topic has been closed for replies.
Best answer by Pavel A.

For testing, better use some printable characters rather than codes in control range.

Fore example

char buffer[] = "test";

HAL_UART_Transmit(&huart2, (void*)buffer, strlen(buffer), 1000);

-- pa

2 replies

Pavel A.
Pavel A.Best answer
May 4, 2019

For testing, better use some printable characters rather than codes in control range.

Fore example

char buffer[] = "test";

HAL_UART_Transmit(&huart2, (void*)buffer, strlen(buffer), 1000);

-- pa

andreaspiezia9
Associate III
May 4, 2019

Thanks a lot Pavel! Now works good.