Senior
May 4, 2019 2:59 PM UTC
Question
TouchGFX 4.10.0 with STM32CubeIDE 1.0.0 and STM32F476G-Disco
- 11 replies
- 4112 views
Not really a question. I have attached a little test project for the STM32F476-Disco board using the newest ST tools. There are still problems and changes need to be made to the project. The Simulator and Build Code buttons do not work in the designer. The TouchGFX command line tool must be used for building the objects and the simulator. The simulator.exe file is located in the build folder within the TouchGFX folder. Before loading it into the target the code must be build with STM32CubeIDE.