2019-05-02 2:02 AM
Hello all,
I will replace Texts on a running device. I'm using a STM32F7 and a external Flash to store Texts, Fonts and Bitmaps. For different variants of the device, we have to replace some of these Texts, Fonts and Bitmaps in the production line.
The problem is that the new text can be longer or shorter than the old text. Of that reason the address of each texts in the Flash are different.
I'm looking for a solution to change texts and replace the start addresse of the Text section, on a running device.
So here my questions:
Thanks for help
Solved! Go to Solution.
2019-12-11 2:39 AM
2019-05-03 3:55 AM
Hi @ARied,
The upcoming version of TouchGFX (4.11.0) will support what you're asking: Dynamic texts/translations. It is not a trivial thing to do in 4.10.0. Stay tuned!
Best regards,
Martin
2019-05-03 4:41 AM
Thanks for the answer Martin.
Can you say, when TouchGFX 4.11 will be available?
2019-05-03 4:52 AM
I can't, other than it's ready to ship, but we're waiting for other internal projects to be ready. Sorry.
I will try to let you know when it ships.
/Martin
2019-12-11 2:17 AM
Hello Martin,
Hello Community,
You said: The upcoming version of TouchGFX (4.11.0) will support what you're asking: Dynamic texts/translations. Now 4.12.3 is available.
Can you explain OR give me a hint, how the dynamic text usage/replacement can be realised?
Thanks
Andreas
2019-12-11 2:39 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.