Skip to main content
SPare.9
Associate
April 30, 2019
Question

Not able to wake stm32476 from deep-sleep (stop2) using EXTI on GPIO

  • April 30, 2019
  • 1 reply
  • 1029 views

Hi,

I am working on "Deep sleep" and "Wake- Up" on STM32L476 MCU. It looks like that MCU is going in to Deep Sleep (STOP2) mode, but I am not able to "wake up" using the GPIO EXTI (GPIO External Interrupts). Following the code snippets, which I am using to put the MCU in deep sleep mode (STOP2) mode, and I am generating the external interrupt on one of the GPIO pin ( note that the interrupt call back "HAL_GPIO_EXTI_Callback" is getting called when the CPU is working normally , before I put into Deep sleep mode)

void put_mcu_deepsleep_mode(void)

{

//Disabling few peripherals to save more power

   HAL_UART_DeInit(&huart3);

   HAL_UART_DeInit(&huart4);

   HAL_UART_DeInit(&huart1);

   HAL_UART_DeInit(&huart5);

   HAL_SPI_DeInit(&hspi3);

   HAL_TIM_Base_DeInit(&htim3);

   HAL_TIM_Base_DeInit(&htim5);

   HAL_GPIO_WritePin(GPIOC, MPU_EN_Pin, GPIO_PIN_RESET);

   HAL_GPIO_WritePin(GPIOC, SUB1_PWR_EN_Pin, GPIO_PIN_RESET);

   HAL_GPIO_WritePin(GPIOA, LIN_EN_Pin, GPIO_PIN_RESET);

  /* Clearing the bit as per the reference manual to enter into STOP2 mode"

   CLEAR_BIT(PWR->CR1, PWR_CR1_LPR);

   osDelay(1000); /* Put delay before going to shut down */

   /* Enter stop2 mode */

   HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

}

Also note that I have tired following as an alternate option to check if I can wake up the MCU using EXTI on GPIO. But couldn't able to wake up.

void put_mcu_deepsleep_mode(void)

{

HAL_EnableDBGStopMode();

/* Disable WKUP pin */

HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN1 );

HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN2 );

HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN3 );

HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN4 );

HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN5 );

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

/* Enable WKUP pin */

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2);

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN3);

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4);

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN5);

__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI);

 osDelay(1000); /* Put delay before going to shut down */

HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON,PWR_STOPENTRY_WFI);

}

This topic has been closed for replies.

1 reply

Mohamed Aymen HZAMI
ST Employee
May 17, 2019

Hello,

Are you using an EXTI or wake-up pin as wake-up event ?

Best Regards,

Mohamed Aymen.